Skip to main content
carlogulliani
Associate III
September 15, 2020
Question

How to implement micros() function on stm8s003?

I need to decode ASK/OOK signal, for this aim I need to know the period in microseconds between several edges. I decided to use TIM1 for this purpose, here is my code

 // Set fCPU = 16MHz
 CLK_CKDIVR = 0;
 CLK_PCKENR1 = 0xFF;
 CLK_PCKENR2 = 0;
 
uint16_t micros() {
 return (uint16_t) ((TIM1_CNTRH << 8) | TIM1_CNTRL);
}
 
void tim1_init(void) {
 // 1MHz = 1uS
 TIM1_PSCRH = 0x00;
 TIM1_PSCRL = 0x10;
 
 TIM1_IER = 0x00; // disable interrupts
 TIM1_CR1 = 0x01;
}

and to get signal I use

ISR_PORTD(handlerD) {
	state = PinRead(GD0_PORT, GD0_PIN);
 uint16_t m = micros();
 if (state == HIGH) {
 lolen = abs(m - prevtime);
 }
 else {
 hilen = abs(m - prevtime);
 }
 prevtime = abs(m);
 if (state == HIGH)
 {
 if (flag == 0) {
 // the end of packet
 if (CheckValue(Pe, hilen) && CheckValue(Pe2, lolen)) // valid 1
 {
 if (bcounter < 32)
 code1 = (code1 << 1) | 1;
 else if (bcounter < 64)
 code2 = (code2 << 1) | 1;
 bcounter++;
 }
 else if (CheckValue(Pe2, hilen) && CheckValue(Pe, lolen)) // valid 0
 {
 if (bcounter < 32)
 code1 = (code1 << 1) | 0;
 else if (bcounter < 64)
 code2 = (code2 << 1) | 0; bcounter++;
 }
 else
 bcounter = 0;
 }
 else {
 if (bcounter < 32)
 code1 = (code1 << 1) | 1;
 else if (bcounter < 64)
 code2 = (code2 << 1) | 1;
 bcounter++;
 }
 }
 //printf("bcounter: %d\r\n", bcounter);
 if (bcounter >= 65)
 {
 printf("Got: %x %x\r\n", code1, code2);
 Pe2 = lolen;
 Pe = hilen;
 flag = 1;
 bcounter = 0;
 code1 = 0;
 code2 = 0;
 }
}

but get the values not I expected

    This topic has been closed for replies.