Skip to main content
jeffrey2
Associate II
Jan 7, 2010 8:33 AM UTC
Question

How to design NEC IR decoder in STM8S103F3 ?

Posted on January 07, 2010 at 09:33

How to design NEC IR decoder in STM8S103F3 ?

#remote #nec #ir
    This topic has been closed for replies.

    9 replies

    jeffrey2
    jeffrey2Author
    Associate II
    May 17, 2011 1:06 PM UTC
    Posted on May 17, 2011 at 15:06

    Quote:

    On 15-12-2009 at 10:15, Anonymous wrote:

    Quote:

    Are there any STM8S103 reference design or technical information for reference ?

    It's all here:

    http://www.st.com/mcu/modules.php?name=mcu&file=familiesdocs&FAM=113

     

    Are there any application notes which describe the TV NEC IR decoder

    design in STM8S MCU ?

    st3
    Associate III
    May 17, 2011 1:06 PM UTC
    Posted on May 17, 2011 at 15:06

    Quote:

    Are there any STM8S103 reference design or technical information for reference ?

    It's all here:

    http://www.st.com/mcu/modules.php?name=mcu&file=familiesdocs&FAM=113

     

    jeffrey2
    jeffrey2Author
    Associate II
    May 17, 2011 1:06 PM UTC
    Posted on May 17, 2011 at 15:06

    I am designing a battery-based device.

    It stayed power down mode normally and

    is powered on by NEC remoter controller.

    Are there any STM8S103 reference design or

    technical information for reference ?

    Thanks in advance !

    selva
    Visitor II
    May 17, 2011 1:06 PM UTC
    Posted on May 17, 2011 at 15:06

    Hi Jeffrey,

    You want to implement an IR transmitter? or receiver?

    regards

    skuk

    mozra27
    Visitor II
    May 17, 2011 1:06 PM UTC
    Posted on May 17, 2011 at 15:06

    Hi Jeffrey,

    You can refer to the ''AN2957: Implementing an RC5 infrared transmitter using the IR timer modulator of the STM8L10x microcontroller'' available in this link:

    http://www.st.com/mcu/familiesdocs-120.html

    This Appli note use the IRTIM IP that is not available on the STM8S products family but can be updated using the Timer ;)

    regards

    mozra

    krzysio
    Visitor II
    May 17, 2011 1:06 PM UTC
    Posted on May 17, 2011 at 15:06

    Hi Boltnut,

    are you writing in C or ASM?

    could you show me your code?

    i'm working on rc receiver too?

    selva
    Visitor II
    May 17, 2011 1:06 PM UTC
    Posted on May 17, 2011 at 15:06

    Hi,

    Am new to STM8 family! and my plan to use Timer1 function to decode NEC IR pulses is on hold for the below reason:

     

    I configured myself every register according to ref manual RM0016 (14587.pdf), section 17.5.3.

    Also have chosen PIO config as alternate input with interrupt on DDR, CR1, CR2.

    There is an interrupt raised on press of the key, but the CC1IF bit is not set, instead, the register is always 0x19, which is to say CC4IF, CC3IF.

    That didn’t help!

    I managed to dig out the reference code on timer, stm8s_tim1.c, and used that as well. Still the same effect

    This makes me think, perhaps I have missed to set/reset just “one bit� somewhere!

    If you could share me your thoughts and further check points or some source code to refer to, that would be appreciated.

    Many thanks,

    Skuk.
    jeffrey23
    Associate III
    May 17, 2011 1:06 PM UTC
    Posted on May 17, 2011 at 15:06

    I had implemented the NEC IR receiver using PC.6,

    but it may be conflicted with other signal (PC.3).

    They shared the same EXTI_PORTC_ISR

    interrupt service routine. How to distinguish them

    in ISR ?

    jeffrey23
    Associate III
    May 17, 2011 1:06 PM UTC
    Posted on May 17, 2011 at 15:06

    Hi wojcik.krzysztof,

    I had implemented the NEC IR decoder (PC.6) in STM8S103F3, but

    it is disturbed by other signal (PC.3). So far I do NOT know

    how to distinguish the EXTI Port C pins interrupt sources to overcome

    the issue.