Skip to main content
Tk.2
Visitor II
October 26, 2020
Question

How to configure Timer for STM8s as input capture compare and how to get the capture compare values in interrupt handler.?

I have configured the timer as below is its is correct and also in interrupt handler I am not getting time the values.

static void TIM3_Config(void)

{

 /* TIM3 configuration:

  - TIM3CLK is set to 16 MHz, the TIM2 Prescaler is equal to 16 so the TIM2 counter

  clock used is 16 MHz / 16 = 1 000 000 Hz

 - With 1 000 000 Hz we can generate time base:

   max time base is 256us if TIM2_PERIOD = 255 --> (255 + 1) / 1 000 000 = 256us

   min time base is 1us  if TIM2_PERIOD = 1  --> ( 1 + 1) / 1 000 000 = 2us

 - In this example we need to generate a time base equal to 10us

  so TIM2_PERIOD = (0.000010 * 1000000 - 1) = 9 */

  

 /* Time base configuration */

 //TIM3_DeInit();//me 

 //TIM3_TimeBaseInit(TIM3_PRESCALER_16 , 9);

  

 /* Config channel1 as input capture */

 //TIM3_ICSELECTION_TRGI

 TIM3_ICInit(TIM3_CHANNEL_2,TIM3_ICPOLARITY_RISING,TIM3_ICSELECTION_DIRECTTI,TIM3_ICPSC_DIV8, 0);//TIM3_CHANNEL_1//TIM3_ICPSC_DIV2

  

 /* Clear TIM2 update flag */

 TIM3_ClearFlag(TIM3_FLAG_CC2);//TIM3_FLAG_CC1

 /* Enable update interrupt */

 TIM3_ITConfig(TIM3_FLAG_CC2, ENABLE);//TIM3_IT_CC1

 //------------------------------------------------------------

 TIM3_UpdateRequestConfig(TIM3_UPDATESOURCE_REGULAR);//UPDATED

// TIM3->IER &= ~TIM3_IER_CC2IE;//Disable OC Compare

// TIM3->SR1 &= ~TIM3_SR1_CC2IF;//Clear Capture comapre flag

 TIM3->IER |= TIM3_IER_CC2IE;//Enable Capture Compare

 //-------------------------------------------------------------

 TIM3_ClearITPendingBit(TIM3_FLAG_UPDATE);//added//TIM3_IT_CC2//TIM3_IT_UPDATE //TIM1_ClearFlag(TIM1_FLAG_CC1 | TIM1_FLAG_UPDATE);

 /* enable interrupts */

 enableInterrupts();

 /* Enable TIM2 */

 TIM3_CCxCmd(TIM3_CHANNEL_2, ENABLE);

 //TIM3_GenerateEvent(TIM3_EVENTSOURCE_CC2);

 TIM3_Cmd(ENABLE);

}

///------------------------Interrupt Handelr--------------------

if((TIM3->SR1 & TIM3_FLAG_CC2)!=0)//sr1

 {   

  if(numberofcapture==0)

  {

    t1 = TIM3_GetCapture2();

    // count_ms1=TIM3_GetCapture2();   //First Capture

    numberofcapture=1;

    // TIM3_ClearFlag(TIM3_FLAG_CC2);

  }

  else 

  {

    t2 = TIM3_GetCapture2();      //Second Capture

    numberofcapture=0;

     

  }

  TIM3_ClearFlag(TIM3_FLAG_CC2);

  count_ms1 = ((t2 - t1));

}

}

Is this is correct to configure the timer to get the values as capture compare..?

----------------------------------Please Help------------------------------

    This topic has been closed for replies.

    1 reply

    JAhme.2
    Visitor II
    January 19, 2022

    Did you resolve this issue ?