Skip to main content
MCuli.1
Associate
February 23, 2022
Question

How to clear/reset timer WITHOUT generating/setting UIF flag??

In documentation for timers on S103/S105/S003 it says that bit URS or register TIMx_CR1 should allow that CNTR=x or EGR |= UG update the timer counter WITHOUT setting the UIF flag:

TIM2:

URS: Update request source

0: When enabled by the UDIS bit, the UIF bit is set and an update interrupt request is sent when one

of the following events occurs:

–

Registers are updated (counter overflow/underflow)

–

UG bit is set by software

–

Update event is generated through the clock/trigger controller

1: When enabled by the UDIS bit, the UIF bit is set and an update interrupt request is sent only when

registers are updated (counter overflow/underflow).

TIM4:

URS: Update request source

0: When enabled, an update interrupt request is sent as soon as registers are updated (counter

overflow).

1: When enabled, an update interrupt request is sent only when the counter reaches the

overflow/underflow.

I'm not sure if USR bit is only "active" if UDIS is active too - but that make not much sense to me.

Anyway, I would like to clear/reset a timer (TIM4) as fast as possible without setting UIF flag.

It's a time critical part and consuming 3 instructions just to reset the timer is not really acceptable. (by setting UDIS=1, CNTR=x, UDIS=0)

Shouldn't the USR bit control if UIF if set ONLY by counter overflow/underflow or by any counter update?

Any ideas on how to just clear/reset the timer as fast as possible?

It's used as a kind of "watchdog" but without interrupts (too slow)

Regards,

    This topic has been closed for replies.