Question
How to add constant voltage and constant current circuit in VIPER35 based SMPS design
- 2 replies
- 2225 views
Hello, I want to design the SMPS (Isolated fly back with opto coupler) have output of 10V and 1.5A (i.e 15W) with constant voltage (CV) and constant current (CC) with input range 90V to 265V, 50Hz, i selected VIPER35HD chip for this design with eDesignSuite, but not able to added the CV/CC in the design input specification, because we need CC to charge the Li-Ion battery. Can someone help, how i can add the CV/CC in edesignsuite.