Skip to main content
Nandish Jasani
Associate
Sep 21, 2018 1:42 PM UTC
Question

How global variable defines in COSMIC C Compiler for STM8S?

Hi,

How can i define global variable in COSMIC C Compiler for STM8S? Is there any document which can explain for global variable definition in COSMIC C Compiler?

Regards,

Nandish Jasani.

    This topic has been closed for replies.

    3 replies

    Philipp Krause
    Senior II
    Sep 23, 2018 2:42 PM UTC

    There is nothing Comsic-specific here. It works just as in any other C compiler: Any variable declared at file-scope that does not have static storage is global.

    Philipp

    Nandish Jasani
    Associate
    Sep 24, 2018 4:59 AM UTC

    Thanks Philipp for your reply,

    Actually i have main.h file where i define some constants and function declarations. I include this file in my main.c program. But in main.h file when i define constant array variable, compiler gives the error. Below is the error in Cosmic Compiler.

    In fact any variable i defined in main.h file, compiler gives error of multiply defined.

    Is there any way to solve this issue?

    [#error clnk Debug\tsd.lkf:54 Debug\main.o: symbol _sddds multiply defined (Debug\stm8s_it.o)

     The command: "clnk -m Debug\tsd.map -l"C:\Program Files (x86)\COSMIC\FSE_Compilers\CXSTM8\Lib" -o Debug\tsd.sm8 Debug\tsd.lkf " has failed, the returned value is: 1

    exit code=1.]

    Below is the main.h and main.c file.

    Regards,

    Nandish Jasani.

    // This is main.h file
     
    #include <iostm8s.h>
    #include <stm8s_it.h>
     
    #define HSE 				0xb4
    #define LSI 				0xd2
    #define HSI 				0xe1
    #define F_CPU				16000000UL
     
    #define RIM 				_asm("rim")
    #define SIM 				_asm("sim")
     
    void ControllerInitialization(void);
    void WatchDogInitialization(void);
    void SwitchClockSourceToHSE(void);
    void WatchDogReset(void);
    void DIOConfiguration(void);
    void Timer4Initialization(void);
    void Delay250uSecond(void);
    void Delay1mSecond(void);
    void Delay100mSecond(void);
    void Delay250mSecond(void);
    void Delay500mSecond(void);
    void Delay1Second(void);
    void DLEDIOConfiguration(void);
    void SDROWIOConfiguration(void);
    void SDCOLIOConfiguration(void);
    void KEYIOConfiguration(void);
    void ELEVATORIOConfiguration(void);
     
    _Bool 	SWEN 				@CLK_SWCR:1;
    _Bool 	SWBSY 			@CLK_SWCR:0;
    _Bool		ODR3				@PE_ODR:3;
    _Bool		CEN					@TIM4_CR1:0;
    _Bool		UIF					@TIM4_SR:0;
     
    #define	DLED				ODR3
    #define ONDLED			DLED = 0
    #define OFFDLED			DLED = 1
    #define ONTIM4			CEN = 1
    #define OFFTIM4			CEN = 0
    #define CLRTIM4INT	UIF = 0
     
    const unsigned char sddds[100][8] = 
    {
    	{0xc7, 0xbb, 0xbb, 0xbb, 0xbb, 0xbb, 0xbb, 0xc7},
    	{0xef, 0xcf, 0xef, 0xef, 0xef, 0xef, 0xef, 0xc7},
    	{0xc7, 0xbb, 0xfb, 0xfb, 0xf7, 0xef, 0xdf, 0x83},
    	{0xc7, 0xbb, 0xfb, 0xe7, 0xfb, 0xfb, 0xbb, 0xc7},
    	{0xfb, 0xf3, 0xeb, 0xdb, 0xbb, 0x83, 0xfb, 0xfb},
    	{0x83, 0xbf, 0xbf, 0x81, 0xfb, 0xfb, 0xbb, 0xc7},
    	{0xc7, 0xbb, 0xbf, 0x87, 0xbb, 0xbb, 0xbb, 0xc7},
    	{0x83, 0xfb, 0xfb, 0xf7, 0xef, 0xdf, 0xdf, 0xdf},
    	{0xc7, 0xbb, 0xbb, 0xc7, 0xbb, 0xbb, 0xbb, 0xc7},
    	{0xc7, 0xbb, 0xbb, 0xbb, 0xc3, 0xfb, 0xbb, 0xc7},
    							
    	{0xb9, 0x36, 0xb6, 0xb6, 0xb6, 0xb6, 0xb6, 0x19},
    	{0xbb, 0x33, 0xbb, 0xbb, 0xbb, 0xbb, 0xbb, 0x11},
    	{0xb9, 0x36, 0xbe, 0xbe, 0xbd, 0xbb, 0xb7, 0x10},
    	{0xb9, 0x36, 0xbe, 0xb9, 0xbe, 0xbe, 0xb6, 0x19},
    	{0xbe, 0x3c, 0xba, 0xb6, 0xb6, 0xb0, 0xbe, 0x1e},
    	{0xb0, 0x37, 0xb7, 0xb1, 0xbe, 0xbe, 0xb6, 0x19},
    	{0xb9, 0x36, 0xb7, 0xb1, 0xb6, 0xb6, 0xb6, 0x19},
    	{0xb0, 0x3e, 0xbe, 0xbd, 0xbb, 0xbb, 0xbb, 0x1b},
    	{0xb9, 0x36, 0xb6, 0xb9, 0xb6, 0xb6, 0xb6, 0x19},
    	{0xb9, 0x36, 0xb6, 0xb6, 0xb8, 0xb1, 0xb6, 0x19},
    							
    	{0x99, 0x66, 0xe6, 0xe6, 0xd6, 0xb6, 0x76, 0x09},
    	{0x9b, 0x63, 0xeb, 0xeb, 0xdb, 0xbb, 0x7b, 0x01},
    	{0x99, 0x66, 0xee, 0xee, 0xdd, 0xbb, 0x77, 0x00},
    	{0x99, 0x66, 0xee, 0xe9, 0xde, 0xbe, 0x76, 0x09},
    	{0x9e, 0x6c, 0xea, 0xe6, 0xd6, 0xb0, 0x7e, 0x0e},
    	{0x90, 0x67, 0xe7, 0xe1, 0xde, 0xbe, 0x76, 0x09},
    	{0x99, 0x66, 0xe7, 0xe1, 0xd6, 0xb6, 0x76, 0x09},
    	{0x90, 0x6e, 0xee, 0xed, 0xdb, 0xbb, 0x7b, 0x0b},
    	{0x99, 0x66, 0xe6, 0xe9, 0xd6, 0xb6, 0x76, 0x09},
    	{0x99, 0x66, 0xe6, 0xe6, 0xd8, 0xb1, 0x76, 0x09},
    							
    	{0x99, 0x66, 0xe6, 0x96, 0xe6, 0xe6, 0x66, 0x99},
    	{0x9b, 0x63, 0xeb, 0x9b, 0xeb, 0xeb, 0x6b, 0x91},
    	{0x99, 0x66, 0xee, 0x9e, 0xed, 0xeb, 0x67, 0x90},
    	{0x99, 0x66, 0xee, 0x99, 0xee, 0xee, 0x66, 0x99},
    	{0x9e, 0x6c, 0xea, 0x96, 0xe6, 0xe0, 0x6e, 0x9e},
    	{0x90, 0x67, 0xe7, 0x91, 0xee, 0xee, 0x66, 0x99},
    	{0x99, 0x66, 0xe7, 0x91, 0xe6, 0xe6, 0x66, 0x99},
    	{0x90, 0x6e, 0xee, 0x9d, 0xeb, 0xeb, 0x6b, 0x9b},
    	{0x99, 0x66, 0xe6, 0x99, 0xe6, 0xe6, 0x66, 0x99},
    	{0x99, 0x66, 0xe6, 0x96, 0xe8, 0xe1, 0x66, 0x99},
    							
    	{0xe9, 0xc6, 0xa6, 0x66, 0x66, 0x06, 0xe6, 0xe9},
    	{0xeb, 0xc3, 0xab, 0x6b, 0x6b, 0x0b, 0xeb, 0xe1},
    	{0xe9, 0xc6, 0xae, 0x6e, 0x6d, 0x0b, 0xe7, 0xe0},
    	{0xe9, 0xc6, 0xae, 0x69, 0x6e, 0x0e, 0xe6, 0xe9},
    	{0xee, 0xcc, 0xaa, 0x66, 0x66, 0x00, 0xee, 0xee},
    	{0xe0, 0xc7, 0xa7, 0x61, 0x6e, 0x0e, 0xe6, 0xe9},
    	{0xe9, 0xc6, 0xa7, 0x61, 0x66, 0x06, 0xe6, 0xe9},
    	{0xe0, 0xce, 0xae, 0x6d, 0x6b, 0x0b, 0xeb, 0xeb},
    	{0xe9, 0xc6, 0xa6, 0x69, 0x66, 0x06, 0xe6, 0xe9},
    	{0xe9, 0xc6, 0xa6, 0x66, 0x68, 0x01, 0xe6, 0xe9},
    							
    	{0x09, 0x76, 0x76, 0x16, 0xe6, 0xe6, 0x66, 0x99},
    	{0x0b, 0x73, 0x7b, 0x1b, 0xeb, 0xeb, 0x6b, 0x91},
    	{0x09, 0x76, 0x7e, 0x1e, 0xed, 0xeb, 0x67, 0x90},
    	{0x09, 0x76, 0x7e, 0x19, 0xee, 0xee, 0x66, 0x99},
    	{0x0e, 0x7c, 0x7a, 0x16, 0xe6, 0xe0, 0x6e, 0x9e},
    	{0x00, 0x77, 0x77, 0x11, 0xee, 0xee, 0x66, 0x99},
    	{0x09, 0x76, 0x77, 0x11, 0xe6, 0xe6, 0x66, 0x99},
    	{0x00, 0x7e, 0x7e, 0x1d, 0xeb, 0xeb, 0x6b, 0x9b},
    	{0x09, 0x76, 0x76, 0x19, 0xe6, 0xe6, 0x66, 0x99},
    	{0x09, 0x76, 0x76, 0x16, 0xe8, 0xe1, 0x66, 0x99},
    							
    	{0x99, 0x66, 0x76, 0x16, 0x66, 0x66, 0x66, 0x99},
    	{0x9b, 0x63, 0x7b, 0x1b, 0x6b, 0x6b, 0x6b, 0x91},
    	{0x99, 0x66, 0x7e, 0x1e, 0x6d, 0x6b, 0x67, 0x90},
    	{0x99, 0x66, 0x7e, 0x19, 0x6e, 0x6e, 0x66, 0x99},
    	{0x9e, 0x6c, 0x7a, 0x16, 0x66, 0x60, 0x6e, 0x9e},
    	{0x90, 0x67, 0x77, 0x11, 0x6e, 0x6e, 0x66, 0x99},
    	{0x99, 0x66, 0x77, 0x11, 0x66, 0x66, 0x66, 0x99},
    	{0x90, 0x6e, 0x7e, 0x1d, 0x6b, 0x6b, 0x6b, 0x9b},
    	{0x99, 0x66, 0x76, 0x19, 0x66, 0x66, 0x66, 0x99},
    	{0x99, 0x66, 0x76, 0x16, 0x68, 0x61, 0x66, 0x99},
    							
    	{0x09, 0xe6, 0xe6, 0xd6, 0xb6, 0xb6, 0xb6, 0xb9},
    	{0x0b, 0xe3, 0xeb, 0xdb, 0xbb, 0xbb, 0xbb, 0xb1},
    	{0x09, 0xe6, 0xee, 0xde, 0xbd, 0xbb, 0xb7, 0xb0},
    	{0x09, 0xe6, 0xee, 0xd9, 0xbe, 0xbe, 0xb6, 0xb9},
    	{0x0e, 0xec, 0xea, 0xd6, 0xb6, 0xb0, 0xbe, 0xbe},
    	{0x00, 0xe7, 0xe7, 0xd1, 0xbe, 0xbe, 0xb6, 0xb9},
    	{0x09, 0xe6, 0xe7, 0xd1, 0xb6, 0xb6, 0xb6, 0xb9},
    	{0x00, 0xee, 0xee, 0xdd, 0xbb, 0xbb, 0xbb, 0xbb},
    	{0x09, 0xe6, 0xe6, 0xd9, 0xb6, 0xb6, 0xb6, 0xb9},
    	{0x09, 0xe6, 0xe6, 0xd6, 0xb8, 0xb1, 0xb6, 0xb9},
    							
    	{0x99, 0x66, 0x66, 0x96, 0x66, 0x66, 0x66, 0x99},
    	{0x9b, 0x63, 0x6b, 0x9b, 0x6b, 0x6b, 0x6b, 0x91},
    	{0x99, 0x66, 0x6e, 0x9e, 0x6d, 0x6b, 0x67, 0x90},
    	{0x99, 0x66, 0x6e, 0x99, 0x6e, 0x6e, 0x66, 0x99},
    	{0x9e, 0x6c, 0x6a, 0x96, 0x66, 0x60, 0x6e, 0x9e},
    	{0x90, 0x67, 0x67, 0x91, 0x6e, 0x6e, 0x66, 0x99},
    	{0x99, 0x66, 0x67, 0x91, 0x66, 0x66, 0x66, 0x99},
    	{0x90, 0x6e, 0x6e, 0x9d, 0x6b, 0x6b, 0x6b, 0x9b},
    	{0x99, 0x66, 0x66, 0x99, 0x66, 0x66, 0x66, 0x99},
    	{0x99, 0x66, 0x66, 0x96, 0x68, 0x61, 0x66, 0x99},
    							
    	{0x99, 0x66, 0x66, 0x66, 0x86, 0x16, 0x66, 0x99},
    	{0x9b, 0x63, 0x6b, 0x6b, 0x8b, 0x1b, 0x6b, 0x91},
    	{0x99, 0x66, 0x6e, 0x6e, 0x8d, 0x1b, 0x67, 0x90},
    	{0x99, 0x66, 0x6e, 0x69, 0x8e, 0x1e, 0x66, 0x99},
    	{0x9e, 0x6c, 0x6a, 0x66, 0x86, 0x10, 0x6e, 0x9e},
    	{0x90, 0x67, 0x67, 0x61, 0x8e, 0x1e, 0x66, 0x99},
    	{0x99, 0x66, 0x67, 0x61, 0x86, 0x16, 0x66, 0x99},
    	{0x90, 0x6e, 0x6e, 0x6d, 0x8b, 0x1b, 0x6b, 0x9b},
    	{0x99, 0x66, 0x66, 0x69, 0x86, 0x16, 0x66, 0x99},
    	{0x99, 0x66, 0x66, 0x66, 0x88, 0x11, 0x66, 0x99},
    };
    // This is main.c file
     
    #include <main.h>
     
    void main(void)
    {
    	ControllerInitialization();
    	WatchDogInitialization();
    	SwitchClockSourceToHSE();
    	Timer4Initialization();
    	ONTIM4;
    	RIM;
    	while (1)
    	{ 
    		WatchDogReset();
    	}
    }
     
    void ControllerInitialization(void)
    {
    	CFG_GCR = 0;
    	FLASH_CR1 = 0x08;
    	RST_SR = 0xff;
    }	
     
    void WatchDogInitialization(void)
    {
    	IWDG_KR = 0x55;
    	IWDG_PR = 3;
    	IWDG_RLR = 0xff;
    	IWDG_KR = 0xcc;
    }
     
    void WatchDogReset(void)
    {
    	IWDG_KR = 0xaa;
    }
     
    void SwitchClockSourceToHSE(void)
    {
    	SWEN = 1;
    	CLK_SWR = HSE;
    	while (CLK_SWR != CLK_CMSR){ WatchDogReset(); }
    	while (SWBSY){ WatchDogReset(); }
    }
     
    void Timer4Initialization(void)
    {
    	TIM4_CR1 = 0x04;
    	
    	// CLK_CNT = fmaster/2^(TIM4_PSCR).
    	// In this case fmaster = 16MHz.
    	// Prescaler is 7 i.e. 128.
    	// CLK_CNT = 16MHz/128 = 125KHz = 8uSec
    	TIM4_PSCR = 0x07;
    	
    	// Auto reload value is 250 i.e. 8uSec * 250 = 2mSec Timer.
    	TIM4_ARR = 250;
    	
    	TIM4_IER = 0x01;
    }
     

    Philipp Krause
    Senior II
    Sep 24, 2018 9:26 AM UTC

    I suggest:

    Put an extern declaration into the .h file:

    extern const unsigned char sddds[100][8];

    Move the definition to a .c file.

    Philipp