Skip to main content
ken
Associate III
May 1, 2007
Question

How do I soft unlock sectors?

  • May 1, 2007
  • 1 reply
  • 572 views
Posted on May 01, 2007 at 16:28

How do I soft unlock sectors?

This topic has been closed for replies.

1 reply

ken
kenAuthor
Associate III
May 17, 2011
Posted on May 17, 2011 at 09:42

I have a test board with an STR911FM44. I am using the Segger J-Link probe with the Segger J-Flash-Arm software. I can connect to the board and read memory back, but if I try to program the flash I get an error indicating the program couldn't soft unlock the flash. What are the requirements for soft unlocking? I don't see it in any of the manuals I have downloaded.

I can use the same probe and application to work on the ST910 eval board, so I know the problem is with my board. Any help would be greatly appreciated.

Thanks.