Skip to main content
Visitor II
Aug 15, 2026 6:25 PM UTC
Question

How can I troubleshoot a USB device that is not detected

I am troubleshooting a USB device that is not being detected by my computer. What are the main hardware and software checks I should perform to determine whether the problem is related to the USB connection, drivers, or the device itself?

3 replies

Karl Yamashita
Super User
Aug 21, 2026 9:04 PM UTC

Are you talking about you don’t hear it enumerate and connect to computer or you don’t see the device in the Device Manager?

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
AScha.3
Super User
Aug 22, 2026 7:41 AM UTC

The enumeration is started by the host, as soon as he gets a voltage on a data line from the device.

So check cables and plug first, try a working device there to prove it can work on this cable and connector.

Then check: is your device pulling up the D+ line? Try 1k5 to 3v3 as pullup, the host should begin enumeration and then tell about unknown or defective device connected.

So you can check for connecting and enumeration. All that happens then depends on a working software on the device as it has to answer now the host for a working enumeration.

If you feel a post has answered your question, please click on " Best Answer ".
Gyessine
ST Technical Moderator
Aug 24, 2026 9:30 AM UTC

Hello ​@MarkManson2323 
add to what ​@AScha.3 said
check also the clock frequency is it clean 48MHZ or not
BR
Gyessine

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.