Skip to main content
cgh21
Associate II
May 28, 2012 12:47 AM UTC
Question

How can I programe E2PROM using word mode?

Posted on May 28, 2012 at 02:47

I tried to use the firmware lib to program it ,but failed.

FLASH_Unlock(FLASH_MEMTYPE_DATA);

  

  for(i = 0; i < DataLeng; i=i+4)

  {

   FLASH_ProgramWord(StartAddr + i,(*(u32*)pBuf));

   pBuf= pBuf+4;;

   FLASH_WaitForLastOperation(FLASH_MEMTYPE_DATA);

  }

FLASH_Lock(FLASH_MEMTYPE_DATA);

But when I use program_byte, it sucess. I just want to save time because I need to programe 23 byte at sequence address one time. Thanks!

ChrisChen
    This topic has been closed for replies.

    3 replies

    konay61
    Associate III
    May 28, 2012 1:17 PM UTC
    Posted on May 28, 2012 at 15:17

    Hi Chris,

    It's just because of the mistake of the firmware code, check the FLASH_ProgramWord() function in stm8l15x_flash.c then correct the Address variable type to uint32_t. After all, hope it will be working properly.

    cgh21
    cgh21Author
    Associate II
    Jun 2, 2012 7:00 AM UTC
    Posted on June 02, 2012 at 09:00

    Thanks for your reply,Now it's ok.

    Thanks very much.

    cgha

    cgh21
    cgh21Author
    Associate II
    Jun 2, 2012 7:46 AM UTC
    Posted on June 02, 2012 at 09:46

    But it's very strange, because when I use the logic analyzer to measure the programe time, it's as long as byte programe. It takes about 187ms to write 7 words. So I think uncomment the

    //FLASH->NCR2 &= (u8)(~FLASH_NCR2_NWPRG);  will not enter word programe mode,but still use byte programe mode ?

    Why?

    ChrisChen