Skip to main content
SBelh.1
Associate II
June 17, 2022
Question

Hi Support, Is there a schematic example for STWBC2-HP with single coil configuration? Regards, Samier

..

This topic has been closed for replies.

7 replies

Peter BENSCH
ST Technical Moderator
June 17, 2022

Welcome, @Community member​, to the community!

the data sheet of the STWBC2-HP already contains two example circuits with single coil, see there page 4 and page 5.

Otherwise you will also find an example with multi-coil in the reference design STDES-50W2CWBC. There, two coils are controlled, but this can easily be reduced to one coil by leaving out one branch, i.e. e.g. the lower Qi coil, C410, C412, C415, Q408, Q409.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
SBelh.1
SBelh.1Author
Associate II
June 17, 2022

Hi Peter,

Thanks for your reply.

Yes. But I have other questions:

1/ In this eval board https://www.st.com/en/evaluation-tools/stdes-50w2cwbc.html

you used variable frequency full-bridge configuration, right?

-What changes are required if I want to use fixed frequency configuration?

2/ If I want to use STWBC2-HP with qi1.3, I need to add Stsafe and NFC?

Is there others requirements?

3/ What is the efficiency of STWBC2-HP?

Thanks in advance,

Best Regards,

Samir

SBelh.1
SBelh.1Author
Associate II
June 20, 2022

Hi Peter,

Can you please answer me?

Regards,

Samir

Peter BENSCH
ST Technical Moderator
June 20, 2022

No, I cannot answer the other questions.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
SBelh.1
SBelh.1Author
Associate II
June 20, 2022

Why?

SBelh.1
SBelh.1Author
Associate II
June 20, 2022

Can you please check this with your colleagues?

ST Technical Moderator
January 8, 2024

Dear customer

1/ In this eval board https://www.st.com/en/evaluation-tools/stdes-50w2cwbc.html
you used variable frequency full-bridge configuration, right?
-What changes are required if I want to use fixed frequency configuration?
A:Yes Full bridge, if you want to use fixed frequency, it need speical FW to support this.

2/ If I want to use STWBC2-HP with qi1.3, I need to add Stsafe and NFC?
Is there others requirements?
A: Yes, you need add STSAFE and update to lastest FW.

3/ What is the efficiency of STWBC2-HP?
A: It depend on RX and coil and system efficiency is about 85%.


For more information please refer to STWBC2-HP - Qi-compatible inductive wireless charger power transmitter for up to 100W applications - STMicroelectronics
Please give your company email for future support.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.