Skip to main content
carlossp
Associate II
December 22, 2022
Question

Hi, in SPI it seems to me there is no difference in the way we configure Full Duplex or unidirectional Transmit-only mode. If there is a difference how can I configure one and other?

When in unidirectional Transmit-only mode, how can I use MISO pin as general

purpose I/O whithout disturb the SPI?

Thanks for any help

    This topic has been closed for replies.

    4 replies

    S.Ma
    Principal
    December 23, 2022

    On my STM32L4 experience, in Master mode, when using tx or rx only will cause losing control of SCK generation at some phase of the communication, while in bidir 4 wire mode, you are 100% in sw control (and lag)

    carlossp
    carlosspAuthor
    Associate II
    December 24, 2022

    Hi, good to know about this.

    thanks for the advice.

    S.Ma
    Principal
    December 25, 2022

    To complete the answer, the peripheral works even if some or all of its 4 signals are pin less. On some SPI generstion, there is an mosi miso swap option which didn't function as expected in bidir mode... in case you reach such choice....

    carlossp
    carlosspAuthor
    Associate II
    December 27, 2022

    Thanks. I just received my stm8s103f. I wrote a small program to test but only tomorrow I will put all together.

    Hve a nice 2023!