Skip to main content
AKUMA.2
Associate II
February 27, 2021
Question

Hi, I am using STM8 DIscovery. I wish to connect my own LCD for different application. Can anyone tell, if the mounted LCD is detachable? Or any process to connect external LCD?

I tried conection my LCD with the available header but the mounted LCD and my LCD and showing half half character.

Thanks

Ajeet

    This topic has been closed for replies.

    3 replies

    Peter BENSCH
    ST Technical Moderator
    March 1, 2021

    Yes, of course you can remove the segment LCD from the STM8A-DISCOVERY or from the STM8L-DISCOVERY, as both use the LCD in DIP-28 on socket.

    Good luck!

    When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    AKUMA.2
    AKUMA.2Author
    Associate II
    March 2, 2021
    Hi, Thank you for the answer.
    However, do we need to desolder?
    Or, can we just pull out the LCD from the Socket?
    Regards
    Ajeet
    Peter BENSCH
    ST Technical Moderator
    March 2, 2021

    No need to desolder, the LCD can be pulled out of the socket.

    Please be very careful, however, as the spring contacts of the socket are quite tight and can hold onto the LCD pins like a barb.

    Good luck!

    /Peter

    In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.