Skip to main content
RRozu.1
Visitor II
March 20, 2022
Question

Hey guys, I want to controll motors via joystick. Unfortunately, when I connect joystick to my STM8S103F3 analogue pins it reads 800 in the middle position instead of 512.

As the result, the right side has very short run (it reaches 1023 in one sixth of travel). The same for Y axis, the same with another joystick. Both joysticks work properly with arduino - middle 520 (or so). Is there any (obvious) reason; how can I remedy this?

Thanks!

SOLVED:

I connected +5V pin of the joystick to +3.3V pin of the MCU - works properly now!

    This topic has been closed for replies.