Skip to main content
This topic has been closed for replies.

2 replies

spectrum_hp2004
Associate III
Aug 5, 2004 7:15 AM UTC
Posted on August 05, 2004 at 09:15

Hi

I am trying to flash the code (str71xdemo_gp.axf) to ST Micro's evaluation board MB393B through ARM realView ICE ( JTAG Emulator).

Processor: STR710FZ2T6.

I want to use the embeded (internal) flash.

During the time of flashing I have maintained the following boot settings: ( RAM MApped at 0h)

BOOTEN:1

BOOT0:0

BOOT1:1

I could succesfully flash the code.

Swicthing off the supply, I changed my boot configuration settings to

USER mode ( Flash mapped at 0h) to run the program.

BOOTEN:0

BOOT0:0

BOOT1:0

But I am not finding anything on the LCD Display.

I am not in a position to findout whether the program is correctly booting from internal flash.

Can anybody help me in giving the correct procedure( step-by-step) of

flashing this code, all the necessry H/W settings to be maintained on the board.

Also tell me Is this, the only file ( str71xdemo_gp.axf)I have to use for flashing or any other associated files are required along with this. If so please mention the same.
spectrum_hp2004
Associate III
Aug 5, 2004 11:34 AM UTC
Posted on August 05, 2004 at 13:34

Hi,

With your new code lcd.zip, we were able to flash the code.

As of now, it is working fine.

Thanks and Thank you very much for the timely help.

We need to do some experiments and run our application which we are planning to conduct tomorrow. We will get back to you with the results tomorrow.

Best Regards,

SPEC