Skip to main content
MAnsa.1
Associate III
December 2, 2020
Question

Hello. I want to use GPIO with STM8S003,

after add

stm8s_gpio.c and stm8s_gpio.h and build project, the compiler(Cosmic) tell error

#error cpstm8 main.c:25(15+3) bad struct/union operand

#error cpstm8 main.c:34(14+3) bad struct/union op

    This topic has been closed for replies.

    3 replies

    MAnsa.1
    MAnsa.1Author
    Associate III
    December 2, 2020

    #error cpstm8 main.c:25(8+5) GPIOA undefined

    it's look like somethings not define to project.

    here is remaining part

    Help please.

    Code:

    25:  sw = GPIOA->IDR & 0x06; 

    34:  if ((GPIOA->IDR & 0x02) == 0) 

     sw = GPIOA->IDR & 0x06; 

    WRost.1
    Associate
    December 3, 2020

    Have you included <stm8s.h> ?

    MAnsa.1
    MAnsa.1Author
    Associate III
    December 3, 2020

    when i include stm8s.h

    it show error like this.....

    #error cpstm8 ..\..\..\data manual\stm8s103f3_spl-master\stm8s103f3_spl-master\stm8s103f3_spl-master\inc\stm8s.h:211(26+6) redeclared typedef int8_t

    #error cpstm8 ..\..\..\data manual\stm8s103f3_spl-master\stm8s103f3_spl-master\stm8s103f3_spl-master\inc\stm8s.h:212(26+7) redeclared typedef int16_t

    #error cpstm8 ..\..\..\data manual\stm8s103f3_spl-master\stm8s103f3_spl-master\stm8s103f3_spl-master\inc\stm8s.h:213(26+7) redeclared typedef int32_t

    #error cpstm8 ..\..\..\data manual\stm8s103f3_spl-master\stm8s103f3_spl-master\stm8s103f3_spl-master\inc\stm8s.h:216(26+7) redeclared typedef uint8_t

    #error cpstm8 ..\..\..\data manual\stm8s103f3_spl-master\stm8s103f3_spl-master\stm8s103f3_spl-master\inc\stm8s.h:217(26+8) redeclared typedef uint16_t

    #error cpstm8 ..\..\..\data manual\stm8s103f3_spl-master\stm8s103f3_spl-master\stm8s103f3_spl-master\inc\stm8s.h:218(26+8) redeclared typedef uint32_t

    #error cpstm8 main.c:9(13+12) missing )

    #error cpstm8 main.c:9(23) missing )

    #error cpstm8 main.c:27(2+10) GPIO_Pin_1 undefined

    9: unsigned int PBSW,PBSW1;

    27: PBSW = GPIOA->IDR & 0x02;

    /*!< Signed integer types */

    211; typedef  signed char   int8_t;

    212: typedef  signed short  int16_t;

    213: typedef  signed long   int32_t;

    /*!< Unsigned integer types */

    216: typedef unsigned char   uint8_t;

    217: typedef unsigned short  uint16_t;

    218: typedef unsigned long   uint32_t;

    line 211-218 are available in stm8s.h file