Skip to main content
Jhabi
Associate
January 12, 2020
Question

Hello I'm Using STM8S003F3PU mini-eval Board. My software is STVD and Cosmic. Why My TIM1 don't work truly? It should measure the input signal HIGH_Duration on TIM1_CH1

Hello

I'm Using STM8S003F3PU mini-eval Board. My software is STVD and Cosmic.

Why My TIM1 don't work truly? It should measure the input signal HIGH_Duration on TIM1_CH1 (= PC6) and my led on PA3 turned off. But that's not so. Furthermore, I use debug mode but it doesn't enter my condition( if(duty_cycle_updated))

Part of my code:

 void TIM1_setup(void){
 TIM1_DeInit();
 TIM1_TimeBaseInit(2000, TIM1_COUNTERMODE_UP, 55535, 1);
 TIM1_CCxCmd(TIM1_CHANNEL_1, ENABLE);
 TIM1_ICInit(TIM1_CHANNEL_1, TIM1_ICPOLARITY_RISING, TIM1_ICSELECTION_DIRECTTI, 1, 1);
 TIM1_ITConfig(TIM1_IT_CC1, ENABLE); 
 TIM1_Cmd(ENABLE);
 enableInterrupts();
}

stm8s_it.c:

void TIM1_CH1_CCP_IRQHandler(void){
 if(TIM1_GetFlagStatus(TIM1_FLAG_CC1)) {
 if(state == FALSE) {
 start_time = TIM1_GetCapture1();
 TIM1_ICInit(TIM1_CHANNEL_1, TIM1_ICPOLARITY_FALLING, TIM1_ICSELECTION_DIRECTTI, 1, 1);
 }
 else {
 end_time = TIM1_GetCapture1();
 TIM1_ICInit(TIM1_CHANNEL_1, TIM1_ICPOLARITY_RISING, TIM1_ICSELECTION_DIRECTTI, 1, 1);
 duty_cycle = (end_time - start_time);
							duty_cycle_updated=TRUE;
 }
 state = ~state;
 }
 TIM1_ClearITPendingBit(TIM1_IT_CC1);
 TIM1_ClearFlag(TIM1_FLAG_CC1);
}
 

Full project attached.

This topic has been closed for replies.

1 reply

Jhabi
JhabiAuthor
Associate
January 12, 2020
Main.c:
 
 #include "stm8s.h"
 
 
 //Pulse width measurment
 unsigned char data_value;
 unsigned long duty_cycle = 0;
 unsigned long duty_cycle_temp = 0;
 
 unsigned long start_time = 0;
 unsigned long end_time = 0;
 bool duty_cycle_updated=FALSE;
 bool state=FALSE;
 void clock_setup(void);
 void GPIO_setup(void);
 void TIM1_setup(void);
 void TIM2_setup(void);
 void delay_cycles(uint16_t cy);
 
 void main() {
 //Set PinMode
 
 GPIOA->DDR |= 0xFF; // PD.0 as Output
 GPIOA->CR1 |= 0xFF; // PD.0 as Push Pull Type Output
 		 GPIOA->ODR |=1ODR &= ~(1