Skip to main content
Stefan Balck
Associate
Nov 17, 2017 1:08 PM UTC
Question

Hello, i'm searching for the Source Code for the Eval Board STEVAL-ILD004V2? There is only the compiled Firmware Version. Can anybody help me?

Posted on November 17, 2017 at 14:08

Hello,

i'm searching for the Source Code of the EVAL Board STEVAL-ILD004V2 with STM8S103F2 Controller?

I can only found the compiled Firmware.

Can anybody help me?

Best Regards,

Stefan

#steval-ild004v2-source-code?
    This topic has been closed for replies.

    7 replies

    Tesla DeLorean
    Guru
    Nov 17, 2017 4:02 PM UTC
    Posted on November 17, 2017 at 17:02

    Where code is unavailable it generally means there are licensing, export or NDA issues, you should contain your local sales office or FAE to obtain access.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Stefan Balck
    Associate
    Dec 5, 2017 1:02 PM UTC
    Posted on December 05, 2017 at 13:02

    Hi Clive One,

    thanks for your answer.

    Now I put the board into operation but it does not work.

    Can it be that the STM8S103F2 is not yet programmed?

    Will the board be delivered unprogrammed?

    The onboard Led is always dark.

     What can i do?

    maurice duteau
    Visitor II
    Apr 12, 2018 7:00 AM UTC
    Posted on April 12, 2018 at 09:00

    We are also looking for the source code. No support from the local ST reps here in Shanghai, been calling several times but nobody picks up. 

    Akshat JAIN_O
    Visitor II
    Apr 12, 2018 8:40 AM UTC
    Posted on April 12, 2018 at 10:40

    Hello,

    The user can download the firmware .hex or .s19 file from the below given link.

    STSW-ILD004FW

    http://www.st.com/content/st_com/en/products/embedded-software/evaluation-tool-software/stsw-ild004fw.html

     
    Akshat JAIN_O
    Visitor II
    Apr 12, 2018 8:49 AM UTC
    Posted on April 12, 2018 at 10:49

    Hello,

    I think you can create a account on my.st.com and request for the complete firmware.

    maurice duteau
    Visitor II
    Apr 13, 2018 3:49 AM UTC
    Posted on April 13, 2018 at 05:49

    Yes, I have created the account but don't see anywhere to reach out to ST other than this forum. We called all the listed numbers in Shanghai and they were not helpful at all. The receptionist says we need to give her the name of our contact and since we don't have one so we're stuck. The engineer will go to their office and see if anyone can help today. This is dragging on too long. 

    WMaca
    Associate II
    Jan 14, 2019 7:09 AM UTC

    Hi,

    I am looking for the source code also.

    Is this one a compiled firmware or this can be modified using the IDE?

    Regards,

    Walter