Skip to main content
Siddharth Kachhia
Associate II
Mar 25, 2017 9:03 AM UTC
Question

Hello, I had developed one application using STVD

Posted on March 25, 2017 at 10:03

#include 'Filter.h'

#define Samples 3

#include <math.h>

#include <stdlib.h>

extern unsigned long int data;

long int Result_Previous,Average,;

unsigned char Stable;

void FIR_Filter(unsigned long int Clean)

{

    static unsigned char Index=0;

//    static bit_16 Index1=4000;

    static unsigned long int ADC_Mean[Samples];

    

    unsigned long int Absolute;

    unsigned char Count;

//    Average = Clean>>5;

    Clean >>= 5;

    ADC_Mean[Index] = Clean;

    Average = 0;

    {    

        for(Count=0;Count<Samples;Count++)

        {

            Average+=ADC_Mean[Count];

             }

        Average /= Samples;

    }

    if(Index >= (Samples-1))

        Index=0;

    else

        Index++;

    Absolute = abs(Average - Result_Previous);

    

   if(Absolute <5)

    {

        Average = Result_Previous +((Average - Result_Previous)>>2);

    }

    if(Absolute<3)

        Stable++;

    else

        Stable=0; 

    

    Result_Previous = Average;

//    return (Average);

        data = Average;

}

this is my code in interrupt function.. i think problem with this statement addition in variable not working in interrupt function  ' Average+=ADC_Mean[Count];'

how can addition in that variable??

Help me for this.. Thank you..

    This topic has been closed for replies.

    6 replies

    S.Ma
    Principal
    Mar 25, 2017 2:07 PM UTC
    Posted on March 25, 2017 at 15:07

    Unclear. Interrupt routine should be as short as possible = as little computation as possible.

    What is the signal triggering the interrupt? Which frequency?

    Try to do the minimum in the interrupt, pass the result in a dedicated global register and set a RAM flag (to prevent future interrupts to corrupt the data). The main loop will wait for the flag, grab the data, divide, and clear the flag.

    Siddharth Kachhia
    Associate II
    Mar 27, 2017 7:01 AM UTC
    Posted on March 27, 2017 at 07:01

    Signal triggering is a falling edge and frequency is 2MHz.

    Arlet Ottens
    Associate II
    Mar 25, 2017 2:25 PM UTC
    Posted on March 25, 2017 at 15:25

    If you're modifying global variables inside an interrupt handler, and you want to access them outside, you need to declare them as 'volatile'.