Skip to main content
hardip
Associate
Jan 17, 2015 11:01 AM UTC
Question

Halt Mode of STM8S

Posted on January 17, 2015 at 12:01

Hello Friends,

I am working with STM8S to develop Remote Control.

So, I want that my STM consume low power during halt mode & it will wake up based on GPIOC (switch) Interrupt.

sw press = remote send on command

sw press = remote send off commnad

...

...

 

I uses halt() function which is in <stm8s.h>  library.

During Run time (Continuous Work)  = 20 mA Power Consumption

After halt() function:

During Halt mode = 10 mA Power Consumption.

My Que are :

->>>

only halt() function is enough to use ST in Halt Mode ? or any other Flag need to be set ?

->>> How to maximum power consumption in STM8S (because 10 mA is too much) ? 

Thanks & Regards,

Hardip 
    This topic has been closed for replies.