Skip to main content
Associate II
October 17, 2024
Solved

HAL_Delay is not working properly for stm32 blue pill

i'm trying to run a simple blinking led program on my stm32f103c8t6 (after i run it several times before successfully), and it doesn't work, when i fix the delay in 1000 ms the led is always on, when i decrement it to 100, 200, 300 it's working properly, but whenever i go above 400 ms it's not working:

Monssef_0-1729150589677.pngMonssef_1-1729150612727.png

 

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
October 17, 2024

Hello @Monssef and welcome to the community,

"X" Pill board flavors (Blue/Black .. other colors) are not the product of ST. They don't contain genuine STM32 chips for years but just fake ones.

I suggest you to purchase any of official ST boards such as NUCLEO-F103RB containing genuine STM32 MCUs.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

8 replies

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
October 17, 2024

Hello @Monssef and welcome to the community,

"X" Pill board flavors (Blue/Black .. other colors) are not the product of ST. They don't contain genuine STM32 chips for years but just fake ones.

I suggest you to purchase any of official ST boards such as NUCLEO-F103RB containing genuine STM32 MCUs.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
MonssefAuthor
Associate II
October 17, 2024

okeyy, but i think all the mcu chips are manufactured by ST because i got already one in a custom pcb and i will rerun the same program in it (even i will struggle to access the pins because i have only the interfaces needed in my project)

thank you !

 

Senior III
October 17, 2024

Can you share the project code? I have webact bluepill stm32f103c8t6. 

"If you feel a post has answered your question, please click ""Accept as Solution""."