Skip to main content
chrisevans3
Associate
Aug 5, 2011 10:26 AM UTC
Question

GPIO struct parameters not initialized

Posted on August 05, 2011 at 12:26

The GPIO struct is defined but it is not initialized before it is used in main.  Everything works but I am stuck with trying to find a value that I can use in GPIO_Init.  GPIOx->CR2 is OR'd with another value and I don't know where to get the initial value GPIOx->CR2.  The only thing I can think is that a random number is in that address.

This is in the given program that comes with the firmware.  I am new to C and this is probably a simple problem. 

Thanks,

Chris

In the main function that comes with the Discovery microcontroller.  The first thing that main does is to call GPIO_Init.   I have included it here.

void GPIO_Init(GPIO_TypeDef* GPIOx,

               uint8_t GPIO_Pin,

               GPIO_Mode_TypeDef GPIO_Mode)

{

 

 

  /*----------------------*/

  /* Check the parameters */

  /*----------------------*/

  assert_param(IS_GPIO_MODE(GPIO_Mode));

  assert_param(IS_GPIO_PIN(GPIO_Pin));

  /* Reset crresponding bit to GPIO_Pin in CR2 register */

  GPIOx->CR2 &= (uint8_t)(~(GPIO_Pin));

  /*-----------------------------*/

  /* Input/Output mode selection */

  /*-----------------------------*/

  if ((((uint8_t)(GPIO_Mode)) & (uint8_t)0x80) != (uint8_t)0x00) /* Output mode */

  {

    if ((((uint8_t)(GPIO_Mode)) & (uint8_t)0x10) != (uint8_t)0x00) /* High level */

    {

      GPIOx->ODR |= GPIO_Pin;

    } else /* Low level */

    {

      GPIOx->ODR &= (uint8_t)(~(GPIO_Pin));

    }

    /* Set Output mode */

    GPIOx->DDR |= GPIO_Pin;

  } else /* Input mode */

  {

    /* Set Input mode */

    GPIOx->DDR &= (uint8_t)(~(GPIO_Pin));

  }

I think you can see that GPIOx->CR2 and GPIOx->ODR and GPIOx->DDR are being used to set bits.(Outlined in RED)  My thinking is that they are not initialized by the function GPIO_Init yet so any number that happens to be in that address could be used.

I am a beginner in both uC's and C.  Thanks for your help.

Chris

#initialize-a-structure #memory-mapped-peripherals
    This topic has been closed for replies.

    5 replies

    Andrew Neil
    Super User
    Aug 6, 2011 7:00 AM UTC
    Posted on August 06, 2011 at 09:00

    Can you show an example to illustrate what you're talking about?

    ''I am new to C''

    Are you also new to programming in general, and/or to microcontrollers, and/or digital electronics?

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    chrisevans3
    Associate
    Aug 8, 2011 4:27 PM UTC
    Posted on August 08, 2011 at 18:27

    Andrew Neil
    Super User
    Aug 9, 2011 6:09 AM UTC
    Posted on August 09, 2011 at 08:09

    ''Thanks for responding to my post.''

    You're welcome. 

    ''I am new to C and uC's''

     

    Don't try to learn too much new stuff all at once!

    It might be easier to learn the 'C' programming language on a PC or other ''normal'' platform before moving on to apply it to microcontrollers...

    Some 'C' starting tips here: 

    http://blog.antronics.co.uk/2011/08/08

    ''have some experience in digital electronics''

    So are you familiar with the concept of memory-mapped IO?

    It means that the IO registers appear in the CPU's normal memory map as normal memory locations - so the CPU accesses the peripherals just with normal memory reads & writes.

    Therefore, by locating 'C' variables at these locations, your 'C' program can access the peripheral registers by just accessing the variables.

    This is what the code you showed is doing - using a struct to group all the registers of a port together.

    Therefore you do not initialise the structure - reading the structure just gives the values from the hardware registers!

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Andrew Neil
    Super User
    Aug 9, 2011 8:36 AM UTC
    Posted on August 09, 2011 at 10:36

    ''memory-mapped IO ... using a struct to group all the registers of a port together''

    Note that this is a very common & widely used technique.

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    chrisevans3
    Associate
    Aug 9, 2011 10:15 AM UTC
    Posted on August 09, 2011 at 12:15