Skip to main content
anil23
Associate III
Sep 22, 2006 6:53 AM UTC
Question

GPIO Speed

Posted on September 22, 2006 at 08:53

GPIO Speed

This topic has been closed for replies.

3 replies

ktchong22
Visitor II
May 17, 2011 7:30 AM UTC
Posted on May 17, 2011 at 09:30

Hi eris,

I am first time using ARM9.

Do you do the same test when running the MCU under the PLL mode (96MHz), and what is your results?

Does it able to perform 96MIPS?

Regards

kais
Associate
May 17, 2011 7:30 AM UTC
Posted on May 17, 2011 at 09:30

Hi Iamanil,

the two code lines inside the while loop takes many cycles, so that the GPIO speed will be quite slow. However if you select the maximum optimization of the IAR tool

your disassembly code will be as follow:

STR R4, [R0, #+0]

STR R6, [R0, #+0]

B 0x000CA4

In this case of optimization, frequency can reach 1.168 KHz.

We can even reach 2.717KHZ if we use the Buffered mode: that means code will be:

while(1)

{

*(u32 *)0x4800A010 = 0x04;

*(u32 *)0x4800A010 = 0x00;

}

Regards.

anil23
anil23Author
Associate III
May 17, 2011 7:30 AM UTC
Posted on May 17, 2011 at 09:30

Hi:

I wrote a simple example to test the maximum speed of the GPIO. All I did was toggle the GPIO pin between 0 and 1. The maximum speed at which the pin was toggling was 400Hz when the MCLK is 32 KHz (RTC oscillator). The code for this example is:

SCU_MCLKSourceConfig(SCU_MCLK_RTC);

for(i = 0; i< 100; i++);

SCU_PLLCmd(DISABLE);

SCU_RCLKDivisorConfig(SCU_RCLK_Div1);

SCU_HCLKDivisorConfig(SCU_HCLK_Div1);

SCU_PCLKDivisorConfig(SCU_PCLK_Div1);

SCU_APBPeriphClockConfig(__GPIO4,ENABLE);

SCU_APBPeriphReset(__GPIO4,DISABLE);

while(1){

*(u8 *)0x5800A010 = 0x00;

*(u8 *)0x5800A010 = 0x04;

}

It’s quite slow to my expectations. Any pointers on this problem would be appreciated.

Regards,