Skip to main content
ryanrsrsrs
Associate II
Feb 15, 2005 2:36 PM UTC
Question

GPIO speed

Posted on February 15, 2005 at 15:36

GPIO speed

This topic has been closed for replies.

2 replies

ryanrsrsrs
Associate II
Feb 15, 2005 12:44 AM UTC
Posted on February 15, 2005 at 01:44

I know the Philips LPC2106 has very slow GPIO. Is the STR711 faster? My application may need to use bit-bang i/o.

If MCLK, PCLK1, PCLK2 all are 48MHz, what will be the execution speed of a string of STR instructions writing to GPIO?

What if MCLK is 48MHz and PCLK1,PCLK2 are both 12MHz?

Will it be faster if the code is executed from sram instead of flash?

ryanrsrsrs
Associate II
Feb 15, 2005 2:36 PM UTC
Posted on February 15, 2005 at 15:36

Thanks for the quick reply. The Philips chip took something ridiculous like 10 cycles!