Skip to main content
sjackson
Associate III
Aug 18, 2008 9:18 AM UTC
Question

GPIO Input Speed

Posted on August 18, 2008 at 11:18

GPIO Input Speed

This topic has been closed for replies.

1 reply

sjackson
sjacksonAuthor
Associate III
May 17, 2011 7:54 AM UTC
Posted on May 17, 2011 at 09:54

I'd like to use the STR9 to help me with a bench test, but I need to know how fast the chip can register changes on GPIO pins configured as inputs. I didn't see any information on this in the data sheet (but maybe I just overlooked it). Does anyone know where there might be a spec on this?

I don't mind running the main clock at 96MHz, but I'd ideally like to be able to detect a pin that changes at about 10MHz.

Thanks.