Skip to main content
nad
Associate III
Dec 22, 2010 10:02 PM UTC
Question

GPIO initialization/testing

Posted on December 22, 2010 at 23:02

hello, 

I just started with the STM8S-discovery .

can you tell me how I boot the pine 0,1,2 port B as input.

and how I'm doing the test on the value entered.

if (?????)

{

    instruction 1....

} 

    This topic has been closed for replies.

    2 replies

    brazov22
    Associate III
    Dec 23, 2010 10:50 AM UTC
    Posted on December 23, 2010 at 11:50

    i.e. for PORTC pin 0:

    #define BUTTON_PORT (GPIOC)

    #define BUTTON_PIN     (GPIO_PIN_0)

    /* -------------------------------------------------------------*/

    /* Check button status */

        if ((GPIO_ReadInputData(BUTTON_PORT) & BUTTON_PIN) == (u8)0x00)

        {

          /* Button is pressed */

          .....

          .....

        }

    by default all ports are configured as input floating. If you want you can configure them as input pull up at the beginning before doing the check on pin port status:

     /* Initialize I/O in Input Mode with pull up and no interrupt*/

      GPIO_Init(BUTTON_PORT, BUTTON_PIN, GPIO_MODE_IN_PU_NO_IT);

    I suggest you to configure it as input pull up so when button is not presd pin0 is high, when you press button pin0 is low.

    brazov2

    nad
    nadAuthor
    Associate III
    Dec 29, 2010 10:05 PM UTC
    Posted on December 29, 2010 at 23:05

    sorry, I made a mistake with the pines. 

    it works now 

    thank you