Getting started with the STUSB4500QTR
- 4 replies
- 2841 views
I'm trying to get started with the STUSB4500QTR and at this point have not changed anything in the device but at the same time I am not using any of its capabilities. The attached schematic shows where I am now. The intent is that a PC (right now just Windows 10) would connect into the 'C' connector and a pigtail connector would carry the D+/D- lines on the the 'C' connector on a Raspberry Pi 4B+. That's what I'm trying to get going now. Eventually, my board (the schematic) would extract power, but that is not my immediate concern.
Right now, if I plug the 'C' cable from the PC directly into the Pi, it works is gadget serial mode - what I want. However, when I plug the PC into my board and the pigtail into the Pi, Windows does not recognize the device.
The pigtail is cut from an 'A' to 'C' adapter cable. The green/white wires are soldered into the test points. The Black and shield are wired in to ground on the PCB. (Red wire is left floating.) All wires are kept as short as possible.
What am I doing wrong? Must there be some setup of the STUSB4500QTR even though the power path is not being used?
Thanks for any pointers.