Skip to main content
wfd
Associate II
Sep 28, 2016 1:36 PM UTC
Question

Getting Cosmic C setup with STVD

Posted on September 28, 2016 at 15:36

I've downloaded STVD, installed it, Downloaded Cosmic C, installed it and downloaded en.stsw-stm8069.zip (standard peripheral library) Now. I cannot for the life of me get this thing working. I opened the .stw project within the unzipped std perph lib and when I build the stm8s105 project I get ''The Executable Cannot be found'' you can fix it by edit...... 

I try and fix it but I have no idea what it wants me to do.

Thanks 

Bill

#stm8s-discovery
    This topic has been closed for replies.

    1 reply

    Ian Legg
    Visitor II
    Sep 29, 2016 9:26 AM UTC
    Posted on September 29, 2016 at 11:26

    Hi Bill,

    When a project is added to the workspace it will ask which toolchain one is using. Alternatively you can set it in Project->Settings (General tab). Obviously the root path needs to be set to where ever you installed the toolchain.

    Hope that helps.

    Thanks,

    Ian