Skip to main content
dotdotdog
Associate II
Dec 16, 2008 4:00 AM UTC
Question

FreeRTOS with ethernet GPIO5

Posted on December 16, 2008 at 05:00

FreeRTOS with ethernet GPIO5

This topic has been closed for replies.

2 replies

sword_82
Visitor II
May 17, 2011 7:57 AM UTC
Posted on May 17, 2011 at 09:57

Hello,

If you need only GPIO5_0 & GPIO5_1 pins, it's not a problem because the Ethernet interface doesn't use them. In other words, you can use the pins 0 and 1 from the Port5 while the Ethernet uses the pins 2 & 3, it's not a problem. But the pins 2 & 3 are mandatory for the Ethernet.

regards

sword

dotdotdog
dotdotdogAuthor
Associate II
May 17, 2011 7:57 AM UTC
Posted on May 17, 2011 at 09:57

Dear,

As mentioned, we need to plug our design board on top of STR91x. But we found a problem, the Ethernet in FreeRTOS on STR91x use the GPIO5 with

GPIO_Struct.GPIO_Pin = GPIO_Pin_2 | GPIO_Pin_3;

......

......

GPIO_InitStructure.GPIO_Alternate = GPIO_OutputAlt2;

but we need the GPIO5 (Pin 0 and Pin 1) to be our extend memory addressing and must be set as:

GPIO_InitStructure.GPIO_Alternate = GPIO_OutputAlt1;

It causes the Ethernet not working at all!! Any solution? Can we use another Pin as Ethernet?

Rickey Leung