Skip to main content
16-32micros
Associate III
Nov 14, 2009 6:22 AM UTC
Question

Flash Loader Demonstrator V2.1.0 Release

Posted on November 14, 2009 at 07:22

Flash Loader Demonstrator V2.1.0 Release

    This topic has been closed for replies.

    1 reply

    16-32micros
    Associate III
    May 17, 2011 1:05 PM UTC
    Posted on May 17, 2011 at 15:05

    Dear Community,

    We are releasing a new STM32â„¢ and STM8â„¢ Flash loader demonstrator that Contains the Demo GUI, Command line and header source files using UART protocol : Version 2.1.0

    http://www.st.com/stonline/products/support/micro/files/um0462.zip

    http://www.st.com/stonline/products/literature/um/13916.pdf

    V2.1.0 - 11/02/2009

    =====================

    New Features

    ************

    + Adding New STM8 map files with options bytes support,

    + Adding ''Echo'' mode option in UART communication for LIN emulation over UART for STM8

    + Adding a new combox with ''No erase'' option when downloading a file.

    Enhancements

    ************

    + Fix of COM ports number > 9 using when using some USB-to-Serial commercial bridges,

    + Fix of --o option (removes FFs data) when using Command line utility,

    + Fix of GUI map files selection in some particular cases,

    + Fix of refresh of the window values after reading Options Bytes,

    + Removing ''Stop Bits'' combox in the GUI first Window,

    + Removing CAN selection over the COMBox bridge board,

    + Removing DFU Selection for the GUI; To use DFU bootloader refer to DFuSe Software,

    + Minor enhancements for dialog box messages and comments for the GUI and Command Line versions.

    Known Limitations

    *****************

    + Automatic selection of some STM8 devices may not work properly.

    If required, use command line version with batch files customization.

    Cheers,

    STOne-32