Skip to main content
qwer.asdf
Senior
Feb 15, 2017 10:09 AM UTC
Question

Fix case sensitvity of HSE_Value in the STM8S_StdPeriph_Lib

Posted on February 15, 2017 at 11:09

In the STM8S_StdPeriph_Lib's stm8.h file there is a section:

#if !defined HSE_Value
 #if defined (STM8S208) || defined (STM8S207) || defined (STM8S007) || defined (STM8AF52Ax) || \
 defined (STM8AF62Ax)
 #define HSE_VALUE ((u32)24000000) /* Value of the External oscillator in Hz*/
 #else
 #define HSE_VALUE ((u32)16000000) /* Value of the External oscillator in Hz*/
 #endif /* STM8S208 || STM8S207 || STM8S007 || STM8AF62Ax || STM8AF52Ax */
#endif /* HSE_Value */�?�?�?�?�?�?�?�?

The first line HSE_Value should be HSE_VALUE because in this way there are no way to override the clock frequency from compiler defines (C is case sensitive language).

Please fix it in the next release! Thank you!

#standard-peripheral-librar #bug #standard-peripheral
This topic has been closed for replies.