Associate II
November 16, 2024
Question
Facing issue in AEK-AUD-C1D9031 AVAS solution board
- 0 replies
- 915 views
Hello everyone, I am using the AEK-AUD-C1D9031 board along with AutoDevKit Studio 2.4.0 for programming. I imported the complete program file from the application library. When I tried to change the sound in the sounddb.s file, the board did not work properly. Since the free UDE license allows a maximum .wav file size of 256 KB, I ensured that my .wav file was around 146 KB. However, the mute LED (D7) glows every time I run the program. I tried pressing and releasing the mute button, which turned off the mute LED, but the sound output was completely unrelated to the .wav file I provided as input. This is the issue I am facing. Kindly share a proper .wav file and example code to test the product completely.