Skip to main content
henrik239955
Associate III
Jun 16, 2005 6:28 AM UTC
Question

External clock DVP3 generates GDI Error

Posted on June 16, 2005 at 08:28

External clock DVP3 generates GDI Error

This topic has been closed for replies.

3 replies

henrik239955
Associate III
Jun 14, 2005 4:36 AM UTC
Posted on June 14, 2005 at 06:36

Hi, I'm using STMDT10-DVP3 and STVD7 3.1.1 to emulate ST7LITE29. When I select FOSC: EXTERNAL the following message appears on screen: ''GDI Error: [10255]''. I have an external 8MHz qrystal connected to OSC1 and OSC2. Whats wrong?

Regards

bood

olivier239955
Visitor II
Jun 15, 2005 4:52 AM UTC
Posted on June 15, 2005 at 06:52

Hi,

When you want to use an external clock you must connect TTL clock signal between EXTCLK pin and GND (see figure 8 of ST7DVP3 user manual attached). The development kit doesn't use the application Crystal connected on OSC1/OSC2 because flat rebbon capacitors can disturb oscillator.

But if you want to use 8MHz frequency you can select it directly with menu: Debug instrument > MCU configuration > Option and chose 8MHz.

With best regards,

________________

Attachments :

st7dvp3.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I05s&d=%2Fa%2F0X0000000bWD%2FBZ.4JuJ3L1z1BuhX8NtFLHTAT.ImWrtvyGF9G5bp9EM&asPdf=false
henrik239955
Associate III
Jun 16, 2005 6:28 AM UTC
Posted on June 16, 2005 at 08:28

Okey, thanks!

/bood