Skip to main content
NS.11
Visitor II
Nov 20, 2018 2:04 PM UTC
Question

Error while compiling

Hi,

I have used the STVD software and the Cosmic C compiler for compiling STM8S003F3P microcontroller. But while compiling I get the error

unknown file type \hstm8

unknown file type +debug

unknown file type -pxp

unknown file type -no

unknown file type -l

unknown file type +mods0

unknown file type -pp

unknown file type -iG:\study\esd\proj\softwares\CXSTM8\Hstm8

unknown file type -clDebug\

unknown file type -coDebug\

 The command: "cxstm8 -i..\softwares\source_include\inc -i..\softwares\en.stsw-stm8069\stm8s_stdperiph_lib\libraries\stm8s_stdperiph_driver\inc -i..\softwares\cxstm8 -i..\softwares\source_include\inc -i..\softwares\en.stsw-stm8069\stm8s_stdperiph_lib\libraries\stm8s_stdperiph_driver\inc \hstm8 +debug -pxp -no -l +mods0 -pp -iG:\study\esd\proj\softwares\CXSTM8\Hstm8 -clDebug\ -coDebug\ main.c " has failed, the returned value is: 1

exit code=1.

main.o - 1 error(s), 0 warning(s)

I have taken the include files and source files from the official page.

Did I miss some file while adding to the project????

    This topic has been closed for replies.