Skip to main content
vaibhav2
Associate II
Aug 6, 2009 2:36 PM UTC
Question

error on touch key example application

Posted on August 06, 2009 at 16:36

error on touch key example application

    This topic has been closed for replies.

    2 replies

    mozra27
    Visitor II
    May 17, 2011 1:04 PM UTC
    Posted on May 17, 2011 at 15:04

    Hi Vaibhav,

    This is a linker issue, that the pragmma section .TSL_IO_ALCODE is declared in the code but not defined in the linker.

    Can you please give me the link to download this project?

    Regards

    mozra

    vaibhav2
    vaibhav2Author
    Associate II
    May 17, 2011 1:04 PM UTC
    Posted on May 17, 2011 at 15:04

    I download the touch key control for stm8 but i got following error while compiling example.stw

    I used cosmic toolchain.

    I am using license for stm8_16k is this error due to that?

    #error clnk Debug\example.lkf:1 no default placement for segment .TSL_IO_ALCODE

    The command: ''clnk -l''C:\Program Files\COSMIC\CXSTM8_16K\Lib'' -o Debug\example.sm8 -mDebug\example.map -sa Debug\example.lkf '' has failed, the returned value is: 1

    exit code=1.

    Please guide me! :o

    Vaibhav