Skip to main content
Srani
Visitor II
March 20, 2019
Question

Error creating process for executable cxstm8 The system cannot find the file specified. Failed to create process.

when i am trying to compile ST Visual develop 4.3.12 with cosmic compiler 4.4.9.0 it is showing

that the executable could not be found you can fix it by editing your too lset settings.

i try to set root path as C:\Program files\cosmic\ fse_compilers\CXSTM8

i am using windows XP and trying to install software again but it showing same error.

please any one help me to solve this problem

    This topic has been closed for replies.

    4 replies

    tvenk
    Associate
    April 5, 2019

    st community please respond to this question i am also facing same problem. can any one help me to solve this?

    AvaTar
    Senior III
    April 5, 2019

    Perhaps very few people use your MCU/toolchain combination ?

    Have you tried to contact Cosmic (FAQs, forum, support) ?

    tvenk
    Associate
    April 8, 2019

    They gave reply like this when i contact cosmic support.

    As you are using STVD which is not a COSMIC’s product, you may contact the ST’s forum.what to do how can i solve this problem.

    ДЕвси.1
    Visitor II
    January 6, 2021

    Hello. For me, the problem was in the template of the Standart peripheral library. The problem was obtained because in the example project include directories SPL was in the folder "Libraries" but in the project includes "libraries" I renamed it and it works. Note:: the libraries must be on 4 levels upper than then project directory (like that ../../../../libraries)