Skip to main content
tvenk
Associate
Mar 19, 2019 9:07 AM UTC
Question

Error creating process for executable cxstm8

I'm using the Cosmic Software 4.4.9.0 in ST Visual Develop 4.3.12  I can't compile it.I try to install again but it showing same error.i tried to set root path correct like this 

C:\Program Files\COSMIC\FSE_compilers\CXSTM8.

Can any one help me to solve this error.

My error is:

---------- Project test - STM8 Cosmic - Configuration Debug -------------

Compiling uartcom\uartcom.c...

cxstm8 +modsl0 +debug -pxp +compact -pp -l -icalibration -ichargercom -iinternal_eeprom -iuartcom -imppt -ispi -i..\pcu1\adc -i"c:\program files\cosmic\cxstm8 -icalibration -ichargercom -iinternal_eeprom -iuartcom -imppt -ispi -i..\pcu1\adc _32k\hstm8" -i"c:\program files\stmicroelectronics\st_toolset\include" -itimer4 -itimer3 -itimer2 -itimer1 -ilcd_lampex -iisr -igpio -iexti -idma -idelay -iclock -ichangeover -iadc -i"C:\Program Files\COSMIC\FSE_Compilers\CXSTM8\Hstm8" -clDebug\ -coDebug\ uartcom\uartcom.c

Error creating process for executable cxstm8

The system cannot find the file specified.

Failed to create process.

test.elf - 1 error(s), 0 2:17 PM 3/19/2019warning(s)

    This topic has been closed for replies.

    1 reply

    AvaTar
    Senior III
    Mar 19, 2019 9:43 AM UTC

    > Error creating process for executable cxstm8

    > The system cannot find the file specified.

    There should be a file cxstm8.exe somewhere in your file system. Is it there ?

    Is the path environment variable set properly ?

    Can you "cd" into said directory, and call it directly on cmd line ?

    > C:\Program Files\COSMIC\FSE_compilers\CXSTM8 ...

    Perhaps you need to put the path string into double quotes, since 'Program Files' contains a space character.