Skip to main content
gendreau
Associate
Dec 7, 2010 12:50 PM UTC
Question

Error 42004 when writing to data flash?

Posted on December 07, 2010 at 13:50

Error 42004 when writing to data flash?

    This topic has been closed for replies.

    3 replies

    gendreau
    gendreauAuthor
    Associate
    May 17, 2011 1:11 PM UTC
    Posted on May 17, 2011 at 15:11

    > you need to copy flash functions in RAM, as specified in FWLIB examples.

    > P.S. In the firs case using FWLIB example remember to set in the linker TAB

    > of STVD the E_W_ROUTs segment as specified in the attached picture.

    Thanks brazov2,

    For some reason I interpreted the documentation to mean that copying the flash write functions to RAM was only necessary when programming the application flash area, not the data flash. Now that I read that paragraph of PM0051 more carefully, this makes perfect sense. I will confirm if this works shortly.

    -helyx

    brazov22
    Associate III
    May 17, 2011 1:11 PM UTC
    Posted on May 17, 2011 at 15:11

    Hi,

    if your application needs a block (128 bytes) to be programmed very quickly (about 4 ms), you need to copy flash functions in RAM, as specified in FWLIB examples. Otherwise you can program a block from eeprom (without loading functions in RAM) writing consecutively 128 bytes without setting any FLASH->CR2 bit. In this latest case the time to program a block is about (128 x 4) ms.

    P.S. In the firs case using FWLIB example remember to set in the linker TAB of STVD the E_W_ROUTs segment as specified in the attached picture.

    brazov2

    gendreau
    gendreauAuthor
    Associate
    May 17, 2011 1:11 PM UTC
    Posted on May 17, 2011 at 15:11

    I have confirmed it. The problem was that I was writing to data flash from a function that was located in program flash.

    The fix in my case (Raisonance compiler) was to add the ''inram'' keyword to the end of the function declaration:

    void FLASH_ProgramBlock(u16 BlockNum, FLASH_MemType_TypeDef MemType, FLASH_ProgramMode_TypeDef ProgMode, u8 *Buffer) inram

    {

        

    ...

    }

    Thank you so much! I was really pulling my hair out on that one.