Skip to main content
ongth60
Associate III
Jun 23, 2005 12:22 PM UTC
Question

error

Posted on June 23, 2005 at 14:22

error

This topic has been closed for replies.

4 replies

ongth60
ongth60Author
Associate III
Jun 18, 2005 1:04 AM UTC
Posted on June 18, 2005 at 03:04

Hi,

Would like to ask y when I run my program Im able to step it but when I run it and stop again, it will state no source for context?

Rgrds,

Ong

ongth60
ongth60Author
Associate III
Jun 18, 2005 5:27 AM UTC
Posted on June 18, 2005 at 07:27

The error stated is

No source for context:

If I take a look at the dissambler, it already jumped to

RO: 00000000 FFFFFFFF DCI 0xffffffff ; ? Undefined.

If I close the RVDK and unplug JTAG and reestablish the link and reopen the project, sometimes I can run the program smoothly.

Pls advise.

Rgrds,

ongth60

ongth60
ongth60Author
Associate III
Jun 21, 2005 10:27 PM UTC
Posted on June 22, 2005 at 00:27

HI,

I've managed to solve the problem.Its due to faulty boot modes. I overlooked the boot modes switches and thought I've set it to RAM :o .

Thanks anyway. Can u pls send me the updated schematic for the JTAG reset circuitry?

Rgrds,

ongth60

kaarthikinfo
Visitor II
Jun 23, 2005 12:22 PM UTC
Posted on June 23, 2005 at 14:22

Hi all,

I am getting the linking error while trying to build my code using ST20R2.0.5 version and the error is ***

''Error-st20link-C:\STM\ST20R2.0.5\lib\os20.lib- symbol _ST_dinkum_setmutexfns not found '' ***

Which we concluded as the symbol definiton was missing in the OS20.lib of this ST20R2.0.5 version.

can anyone suggest me on this issue...

Regards

Kaarthik.