Skip to main content
newsamo
Associate III
Sep 18, 2008 12:24 AM UTC
Question

ERASE FLASH

Posted on September 18, 2008 at 02:24

ERASE FLASH

This topic has been closed for replies.

3 replies

newsamo
newsamoAuthor
Associate III
May 29, 2008 8:28 AM UTC
Posted on May 29, 2008 at 10:28

I'm working on st10f168 with st10flasher, now, load monitor is ok, dump is ok, but i'm not able to program flash because appears error messagea boute flash erase: EraseFlash failed.flash

How can i erase ?

najoua
Associate
Jun 2, 2008 5:05 AM UTC
Posted on June 02, 2008 at 07:05

Hello Newsamo,

Programming voltage (12V) of the on-chip Flash memory must be supplied to pin VPP(pin 84).

Is the 12V ensured in this pin during programming/erasing operation?

Best regards,

Najoua.

joluci
Visitor II
Sep 18, 2008 12:24 AM UTC
Posted on September 18, 2008 at 02:24

Hello Najoua,

in which others microcontrollers of st10fxxx family I need to apply the voltage programming to erase and program?

Thank you !!!