Skip to main content
cyril23
Associate
Jan 20, 2009 5:56 AM UTC
Question

EMC design: How to set TRAP instruction on all unused flash code?

Posted on January 20, 2009 at 06:56

EMC design: How to set TRAP instruction on all unused flash code?

    This topic has been closed for replies.

    3 replies

    cyril23
    cyril23Author
    Associate
    May 17, 2011 1:02 PM UTC
    Posted on May 17, 2011 at 15:02

    Dear All,

    EMC design How to set TRAP instruction on all unused flash code?

    I want to fill unused flash memory with 0x83 (Trap instruction)

    How it is possible with:

    IDE: STVD 4.10

    Compiler Cosmic 4.2.7.

    Thanks

    [ This message was edited by: cyril.rieu on 19-01-2009 17:28 ]

    cyril23
    cyril23Author
    Associate
    May 17, 2011 1:02 PM UTC
    Posted on May 17, 2011 at 15:02

    thanks _luca.

    Solution:

    it is possible to set this option in

    Project->settings->[tab]Linker Category ''input'' at the end of the section name if -m set. and add -f0x83 (filling with trap opcode)

    We obtain this line in lkf file

    +seg .const -b 0x8f00 -m 0xf100 -n .const -it -f0x83

    luca239955_st
    Associate II
    May 17, 2011 1:02 PM UTC
    Posted on May 17, 2011 at 15:02

    look for the -f option in the linker section of the manual: I'm not sure if STVD allows to manage this via the graphical interface, but, worst case, you can edit the .lkf file by hand.

    Regards,

    Luca (Cosmic)