Skip to main content
ken2399
Associate II
May 25, 2012 9:25 PM UTC
Question

Embedded Reference Voltage STM8L151

Posted on May 25, 2012 at 23:25

Hello,

VREFINT is specified as 1.224V +/-20mV with VDD = 3.0V.

Is there any information available on the accuracy when VDD = 1.8V?

Any guidance welcome!!

Kentxu.

#stm8l
    This topic has been closed for replies.

    1 reply

    ken2399
    ken2399Author
    Associate II
    Jun 8, 2012 8:23 PM UTC
    Posted on June 08, 2012 at 22:23

    I guess there's not alot of action in this forum... :(

    If anyone is interested, I've had a reply from ST:

    ''

    Vrefint = 1.224 +/-20mV is guaranteed by characterization on the whole suplly range from 1.65 V to 3.6 V.

    ''

    So that's good news for these parts.