Skip to main content
havard
Associate II
May 26, 2003
Question

Elite Local bus and ATAPI

  • May 26, 2003
  • 3 replies
  • 760 views
Posted on May 26, 2003 at 06:54

Elite Local bus and ATAPI

This topic has been closed for replies.

3 replies

havard
havardAuthor
Associate II
May 21, 2003
Posted on May 21, 2003 at 08:23

Can I use both ATAPI and Local bus at the same time as ATAPI is on ISA bus?

Haavard
stephen239955_st
Associate II
May 23, 2003
Posted on May 23, 2003 at 11:41

No. The ISA and Local Bus are mutually exclusive modes of the STPC. They are selected at the time of the boot and therefore cannot be used at the same time.

thierry239955_st
Associate
May 26, 2003
Posted on May 26, 2003 at 06:54

ATAPI interface is on the PCI bus (not on ISA) and is always available. What is not possible is to have both ISA and Local Bus at the same time.

Farfalla