Skip to main content
Visitor II
July 13, 2025
Question

Efficiency and Power Dissipation of HFDA801L

  • July 13, 2025
  • 1 reply
  • 261 views

We would appreciate it if you could provide information regarding the changes in efficiency and power dissipation (thermal performance) of the HFDA801L under the following conditions:

  • Device: HFDA801L
  • Supply Voltage: 14.4V
  • Input Signal: TDM Fs 48kHz
  • Load: 4 channels × 2Ω (driving 2Ω on all outputs)
  • Planned Register Settings:
    • IB2 D6: "1 – PWM out of phase"
    • IB19 D2: "0 – Slow Slope"
    • IB24 D[1:0]: "01 – PWM Standard Frequency"

We are currently considering the "Slow Slope" setting, but we have some concerns regarding heat generation.
To support our heatsink simulation, we would greatly appreciate it if you could share data showing how efficiency and power dissipation vary between the Slow Slope and Fast Slope settings.

We understand that selecting the Slow Slope may result in lower efficiency.
Thank you very much for your support.

Best regards,

This topic has been closed for replies.

1 reply

ST Employee
July 15, 2025

Hello @Nobu3,

This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.

Best regards,
Maxime

​In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.