Skip to main content
Associate
Apr 29, 2026 10:25 PM UTC
Solved

EEPROM UID and Identification page

I am looking for an EEPROM device that has the UID but also supports the 256-byte identification page.

I was lead to believe that densities less than 1M support either/or, but greaterthan/equal to 1M does support both.

However, from what I can tell from the datasheet(s), the -F version (M24M01E-F) says: "The device offers an additional 256-byte page, called the identification page. This page can be used to store sensitive application parameters, which can later be permanently locked in read-only mode."

But the -F version does not have section 4.5 so it does not have UID.  

datasheet for version -U (M24M01E-U) says "The device also offers an additional 256-byte identification page. This page stores a 128‑bit (16‑byte) unique factory-programmed serial number, locked in read-only mode at factory delivery."

And in section 4.4 says "This is an additional 256-byte page, permanently locked in read-only mode. The user can read it by issuing the read identification page instruction"

Section 4.5 clearly explains UID.

Is there a version that supports storing (and locking) parameters in the 256 identification page AND has the UID? or is it either/or? 

 

Thanks

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Apr 30, 2026 8:16 AM UTC

Welcome @JMAX604, to the community!

Correct, it is either/or.

Background: the Identification Page is present in both cases, but:

  • the one in the M24M01E-F it is user-writable and lockable
  • the one in the M24M01E-U it is preprogrammed by ST with the UID and additionally locked.

At present, STMicroelectronics has no EEPROM in its product range to fulfil your request:

  • one page (r/o + locked) with UID
  • an additional page (r/w + lockable) for your customer-specific identification information

Maybe your requirements and the intended goal can be met with other solutions, such as a device from the family STSAFE?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

Peter BENSCH
Peter BENSCHBest answer
ST Technical Moderator
Apr 30, 2026 8:16 AM UTC

Welcome @JMAX604, to the community!

Correct, it is either/or.

Background: the Identification Page is present in both cases, but:

  • the one in the M24M01E-F it is user-writable and lockable
  • the one in the M24M01E-U it is preprogrammed by ST with the UID and additionally locked.

At present, STMicroelectronics has no EEPROM in its product range to fulfil your request:

  • one page (r/o + locked) with UID
  • an additional page (r/w + lockable) for your customer-specific identification information

Maybe your requirements and the intended goal can be met with other solutions, such as a device from the family STSAFE?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
JMAX604Author
Associate
May 5, 2026 5:44 PM UTC

FYI

The main reason I checked datasheets and posted here is because CoPilot gave me an answer that I wanted to confirm. CoPilot told me that 1M/2M devices can support both (UID/user) but datasheet was pretty clear that they do not.

Glad I checked :)

 

JMAX604_0-1778002972332.png