Skip to main content
jjyeh1976
Associate III
Aug 27, 2009 3:54 PM UTC
Question

EEPROM Read problem

Posted on August 27, 2009 at 17:54

EEPROM Read problem

    This topic has been closed for replies.

    4 replies

    jjyeh1976
    jjyeh1976Author
    Associate III
    May 17, 2011 1:04 PM UTC
    Posted on May 17, 2011 at 15:04

    Hi,

    I follow the example of the firmware libraty to read/write/erase one

    byte of the EEPROM, I can write a byte, but fail to readback, my code

    u8 c;

    u32 add = 0x4000;

    FLASH_SetProgrammingTime(FLASH_PROGRAMTIME_STANDARD);

    FLASH_Unlock(FLASH_MEMTYPE_DATA);

    FLASH_ProgramByte(add, 0xa5);

    c = FLASH_ReadByte((u32)add);

    FLASH_ProgramByte(add,0x5a);

    c = FLASH_ReadByte((u32)add);

    FLASH_EraseByte(add);

    FLASH_ProgramByte(add,0x5a);

    c = FLASH_ReadByte(add);

    I'm sure the FLASH_ProgramByte() executes correctly (I also

    read back using STVP), but the FLASH_ReadByte() always returns

    ''0'', what's wrong?

    Jason

    mozra27
    Visitor II
    May 17, 2011 1:04 PM UTC
    Posted on May 17, 2011 at 15:04

    Hi jason,

    What is the clock speed used in your application? if you use a clock higher than 16MHz you should set the wait state option byte.

    Thanks to verify this point

    regards

    mozra

    jjyeh1976
    jjyeh1976Author
    Associate III
    May 17, 2011 1:04 PM UTC
    Posted on May 17, 2011 at 15:04

    Hi mozra,

    Thanks for your reply.

    I'vd try to read the EEPROM in flash, but failed.

    But I can read the EEPROM in ram.

    regards,

    Jason

    mozra27
    Visitor II
    May 17, 2011 1:04 PM UTC
    Posted on May 17, 2011 at 15:04

    Hi Jason,

    When unlocking the data eeprom you should wait until the DUL flag in the flash status register is set (data eeprom ready),

    FLASH_Unlock(FLASH_MEMTYPE_DATA);

    while (FLASH_GetFlagStatus(FLASH_FLAG_DUL) == RESET);

    if you execute your code from RAM, if the address is in data eeprom memory you should wait until the HVOFF flag in the status register is set (end of high voltage)

    FLASH_ProgramByte(add, 0xa5);

    while (FLASH_GetFlagStatus(FLASH_FLAG_HVOFF) == RESET);

    c = FLASH_ReadByte((u32)add);

    and if the address is in flash program memory you should wait until the EOP flag in the status register is set (End of programming).

    FLASH_ProgramByte(add, 0xa5);

    while (FLASH_GetFlagStatus(FLASH_FLAG_EOP) == RESET);

    c = FLASH_ReadByte((u32)add);

    Normally your code works fine if you use the default clock system HSI/8 (lower execution speed)

    Regards

    mozra

    [ This message was edited by: mozra27 on 26-08-2009 23:11 ]