Solved
ECMF02-2AMX6 GND connection
- 6 replies
- 382 views
Techsupport ignored my request, so I have to come here.
The part is ECMF02-2AMX6. It is CM choke plus ESD surge protector for USB2.
Here's the question: in the datasheet from June 2011 Doc ID 17815 Rev 2, this is the recommended layout is shown (see the image).
As can be seen, pins 3&4 are connected to GND (3 VIAs are being used).
However the Pin 4 is declared "NC". In the text this is not addressed. My request to the support was not answered.
THis is fairly important. If the pin i named "NC", it means "No Connect" unless the opposite openly explained in the text of the datasheet.
Waiting for an answer.