Skip to main content
dmerchez9
Associate III
Apr 12, 2005 6:40 AM UTC
Question

Driver

Posted on April 12, 2005 at 08:40

Driver

This topic has been closed for replies.

3 replies

dmerchez9
dmerchez9Author
Associate III
Apr 7, 2005 11:36 AM UTC
Posted on April 07, 2005 at 13:36

Je dispose d'un STR710FZ2T6

Est ce que j'ai besoin d'un driver pour l'USB ou est qu il fonctionne sans?

Meme question pour l'UART, le CAN et la SmartCard...

Merci

Dam

dmerchez9
dmerchez9Author
Associate III
Apr 11, 2005 3:29 AM UTC
Posted on April 11, 2005 at 05:29

hello

what i want to know is: do i have to use a component loke MAX232 for the UART at the output of the microprocessor?

thanks

dmerchez9
dmerchez9Author
Associate III
Apr 11, 2005 11:01 AM UTC
Posted on April 11, 2005 at 13:01

and what for using USB, CAN, and SC? do they all need driver component?

Dam