Skip to main content
e239955_stm1_stmicro_com
Associate III
Aug 3, 2005 8:27 AM UTC
Question

Downloadind axf file in STR710 eval board

Posted on August 03, 2005 at 10:27

Downloadind axf file in STR710 eval board

This topic has been closed for replies.

4 replies

e239955_stm1_stmicro_com
Associate III
Jul 28, 2005 4:22 AM UTC
Posted on July 28, 2005 at 06:22

Hello,

Is there any software to allow to program the STR710 flash without nedding to create a project?

I'm using the STR710 eval board with Isystem Ione emulator and IAR programming software (my IDE is winIDEA to be complete)

THX

Manu

mivation
Visitor II
Jul 28, 2005 2:07 PM UTC
Posted on July 28, 2005 at 16:07

You can also add your prog.sim simple code programming file to an otherwise empty IAR project. You do this Project>options>linker>extra output.

This is a way to gain the benefit of the IAR bult in JTAG flash programmer via USB JLINK without the cost of segger JFLASH.

I have attached an EWARM 4.30A project to demonstrate programing without source code for an IAR STR711 board via IAR/Segger USB JTAG.

engineer_in_shorts' first posting :)

________________

Attachments :

programmer_only.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtDf&d=%2Fa%2F0X0000000aKQ%2FDp250B49NiuK9skS41QzO9ZE4aifKXr8nIH8KnVjeZw&asPdf=false
e239955_stm1_stmicro_com
Associate III
Jul 29, 2005 6:28 AM UTC
Posted on July 29, 2005 at 08:28

I'm gonna try this,j

thanks for your help

Manu

whhofmeyr
Associate II
Aug 3, 2005 5:12 AM UTC
Posted on August 03, 2005 at 07:12

Hi,

I thought that the .axf files were a proprietary ST version

of .elf format.

Can the third party tools program flash using .axf files?

whh