Skip to main content
heribert
Associate II
Nov 14, 2008 8:40 AM UTC
Question

Download of Main File

Posted on November 14, 2008 at 09:40

Download of Main File

This topic has been closed for replies.

3 replies

heribert
heribertAuthor
Associate II
Sep 8, 2006 8:36 AM UTC
Posted on September 08, 2006 at 10:36

Hello,

there are the good applications ''DfuSeDemo'' and ''Dfu File Manager'' (and all works fine)

I see the *.hex file is converted to *.dfu file, which is (except the first ~100bytes) the same as the *.sim file.

Now are on work to programm our own download software. Is there any documentation available ( e.g. for the application ''DfuSeDemo'').

My question is: what is the start address (first byte) from the download file (*.dfu). What is the requirement for a correct download?

Thanks, Heribert

heribert
heribertAuthor
Associate II
Sep 11, 2006 5:48 AM UTC
Posted on September 11, 2006 at 07:48

Hello,

so i see there is to use the *.bin file for download.

milton
Associate II
Nov 14, 2008 8:40 AM UTC
Posted on November 14, 2008 at 09:40

Hi ! This DfUse application comes with a button to Enter DFU mode/ HID detach and leave DFU mode. Does anyone have a example of a HID firmware with DFU support, I mean a HID/DFU compliant device?