Skip to main content
Associate II
September 2, 2023
Question

Doesn't creating 1us delay by using Timer1 in NUCLEO-F410RBNUF410RB$AU1board.

Hi,

Generated delay of 1 Microsecond in NUCLEO-F410RB board by using Timer1(16bit) with counter but while using Timer(16bit) interrupt mode unable to generate 1 Microsecond delay,even the Pre-scaler,Counter and Clock frequency are at required rate(Counter=10,Prescaler=10,Clock frequency=100Mhz).So verified the NUCLEO-F410RB controller by generating different delay and it generated requireddelays(1s,1ms,10ms,100ms,200μs,100μs) except below 50μs.

 

Thanks &Regards,
M.Gokulraj.
This topic has been closed for replies.

2 replies

Issamos
Super User
September 2, 2023

Hello @Gokulraj 

I suggest you to follow this tutorial to implement your application.

Best regards

II

Tesla DeLorean
Guru
September 2, 2023

You can't interrupt at these high rates.

If you want to measure time have the counter free run at 1 MHz and inspect the count to get the desired delay 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..